Bushing Press: Designed to press bushings into place. It typically consists of a frame, a hydraulic or mechanical press mechanism, and various adapters to accommodate different bushing sizes.
Bushing Driver Set: A collection of cylindrical drivers in various sizes that match the outer diameter of the bushings. They are used with a hammer or mallet to tap the bushing into position.
Bushing Installation Kit: Some bushings may require additional tools for installation, such as bearing or seal drivers. A bushing installation kit usually includes drivers, sleeves, or adapters to accommodate different bushing sizes.
Bench Vise: It can help hold the bushing in place during installation. It provides stability and allows for controlled force when tapping the bushing into position.
Measuring Tools: Measuring tools such as calipers or micrometers are helpful for accurately determining the dimensions of the bushing and its housing.
Importance of Pre-Installation Lubrication
Applying a suitable lubricant to the bushing and mating surface can ease installation. It reduces friction and helps the bushing slide to place smoothly. Use a lubricant compatible with the specific bushing material and the application requirements.
Greases, oil, and dry lubricants make suitable lubricants, such as graphite or molybdenum disulfide. With automated systems, they can be applied manually in an oil bath or mist, and some bushings have lubricant inserts.
Bushing Features that Aid Installation
We recommend installing bushings with an arbor press whenever possible. If the bushing’s OD is large enough, you can use a drawbolt with two washers. If a hammer is the only tool available, do not strike the bushing directly, or it could fracture.
Utilize a soft-metal punch to cushion the blows. Before installing a press-fit bushing, lubricate the inside of the mounting hole and outside of the bushing with a lubricant such as lithium grease. Otherwise, the bushing may score the mounting hole and be difficult to replace later.
The Drill Entrance Radius Feature in Bushings
Bushings feature a blended and polished radius at the drill-entrance end for smooth drill entry and proper alignment, preventing drill wear and breakage. Radius size varies in proportion to drill size.
Importance of Maintaining Bushing Concentricity for Efficient Installation
Bushing concentricity refers to the alignment and centering of a bushing within its intended housing or bore. It is a critical factor in ensuring efficient installation and optimal bushing performance. Concentricity is typically measured by assessing the deviation of the bushing’s centerline from the centerline of the housing or bore.
Concentricity is crucial because it directly affects the bushing assembly’s functionality, reliability, and longevity. It helps in many ways:
Load Distribution: When a bushing is installed concentrically, it helps distribute the load evenly across its entire surface area.
Smooth Operation: Concentricity ensures the bushing rotates or slides smoothly within its housing. Misalignment can result in binding, excessive friction, or jamming, impairing the intended movement of the shaft or component.
Alignment Accuracy: In applications where a bushing supports or guides a shaft or spindle, concentricity plays a critical role in maintaining alignment accuracy.
Reduced Wear and Friction: Concentric bushing installation ensures uniform contact between the bushing and its mating surface, minimizing localized wear and friction.
Sealing and Leakage Prevention: In applications where the bushing acts as a seal or provides a barrier against fluid leakage, concentricity becomes even more critical. Proper alignment ensures an effective seal and prevents bushing and housing leakage.
Tolerances for Bushing Concentricity
Bushing OD is ground concentric to the ID to within.0003 TIR for ID sizes from 1/8 inch to 1/2 inch (3mm to 12mm) unless otherwise indicated.
For larger or smaller sizes, concentricity is within.0005 TIR. Unground bushings are concentric within.006 TIR. On counterbored bushings, concentricity applies only over the drill-bearing length.
Any dimensions without explicitly listed tolerances are held to +/-.015 inches on standard ANSI sizes. Special tolerances for any dimension are available on request as specials.
Key Tolerances to Consider for Bushing Installation
Press-fit Tolerance: Determines the interference or clearance between the bushing and its housing. Achieving the right press fit is crucial to ensure proper load distribution and prevent unwanted movement.
Clearance Tolerance: As mentioned earlier, this refers to the gap between the inner diameter of the bushing and the shaft or pin it accommodates.
Concentricity Tolerance: As mentioned earlier, this refers to the alignment of the bushing’s inner and outer diameters concerning each other. It ensures the bushing is centered within its housing and properly aligns with the shaft.
Surface Finish Tolerance: Determines the roughness or smoothness of the bushing’s inner and outer surfaces. A smooth surface finish reduces friction and wear while also facilitating proper lubrication.
Length Tolerance: This specifies the allowable deviation in the length of the bushing. It ensures the bushing fits properly within its housing without interference or gaps.
Material Thickness Tolerance: If the bushing has any flanges or other features with specific thickness requirements, the material thickness tolerance is the allowable deviation in those dimensions.
Selecting the Appropriate Material for Your Bushing
Drill bushings can come in different materials depending on their application:
Steel: This is a popular choice for drill bushings due to its strength, durability, and resistance to wear. It can withstand high drilling forces and is suitable for various materials.
Bronze: Bronze drill bushings offer good wear resistance and lubricity. They are commonly used in applications requiring low friction and high heat dissipation. Bronze bushings are particularly suitable for drilling materials like aluminum or brass.
Brass is used primarily in applications involving delicate workpieces or materials requiring minimal marring or scratching. Brass bushings offer good corrosion resistance and have low friction properties.
Carbide: Carbide drill bushings are made from tungsten carbide or a similar hard, wear-resistant material. They are ideal for high-speed drilling operations and drilling abrasive or rigid materials such as composites, hardened steels, or ceramics.
Plastic: Plastic drill bushings, often made from materials like nylon or Delrin, are lightweight and offer good resistance to corrosion and chemicals. They are commonly used in applications where weight reduction is essential or when drilling softer materials.
Oil-Impregnated Bronze: Oil-impregnated bronze drill bushings provide self-lubrication during drilling operations. These bushings have tiny pores filled with lubricating oil, reducing friction and extending tool life. They are suitable for high-speed drilling.
Standard drill bushings from Carr Lane Mfg. are made from 1144 Stressproof steel. This material is heat treated to achieve RC 62-64 ID hardness and other high-carbon steels.
Optional materials such as tungsten carbide (Grade C2 carbide with steelhead), 52100 steel, A2 tool steel, D2 tool steel, M2 tool steel, 416 stainless, 440C stainless, 17-4PH stainless, 303 stainless, 660 bronze, Ampco 18 bronze, Ampco 21 bronze, Oilite, and brass are available as specials.
Using a Press Fit Bushings Hole Size Calculator
Use this calculator to determine the proper installation hole size for standard press-fit bushings.
View Calculator