Hydraulic Fluid for Power Workholding Systems
Engineering reference for selecting and specifying hydraulic fluid in KOSMEK Power Workholding installations.
Carr Lane recommends Hangsterfer's Antiwear 32. ISO VG 32, coolant-compatible, formulated for CNC environments where the hydraulic system shares the machine enclosure with water-based cutting fluid.
Order Antiwear 32 from Hangsterfer's →
Overview
Hydraulic power workholding systems installed in CNC machine tools require a hydraulic fluid that performs reliably in a shared machine environment. The dominant operating condition is direct or indirect contact between the hydraulic system and water-based cutting fluid. Seal integrity, actuator response, and long-term system cleanliness all depend on correct fluid selection.
KOSMEK specifies ISO VG 32 hydraulic fluid for all Power Workholding systems. This viscosity grade matches the operating requirements of the hydraulic components used throughout the product line and falls within the performance envelope specified by the system supplier.
Recommended Fluid: Hangsterfer's Antiwear 32
Most ISO VG 32 hydraulic oils on the market will meet the viscosity requirement for KOSMEK Power Workholding systems. What they will not do is protect the cutting fluid in the machine. The moment tramp oil from a standard hydraulic fluid enters the coolant sump, it begins degrading the cutting fluid that tool life and surface finish depend on. That degradation is invisible until the damage is done.
Hangsterfer's Antiwear 32 is the fluid Carr Lane specifies because it solves that problem at the source. It meets the ISO VG 32 requirement and is specifically engineered to reject from water-based cutting fluids rather than emulsify into them. Tramp oil that separates floats to the surface and can be removed; tramp oil that emulsifies cannot. The choice of hydraulic fluid is one of the lowest-cost decisions in a CNC workholding installation and one of the highest-leverage ones for long-term operating cost.
Hangsterfer's has been formulating coolant-compatible machine lubricants since the early 1980s. The Antiwear series meets or exceeds Cincinnati Milacron P-68, P-69, and P-70 specifications and is manufactured under ISO 9001:2015 certification.
Coolant Compatibility: The Critical Selection Criterion
In CNC machining centers, the hydraulic system and the cutting fluid sump occupy the same machine enclosure. Seal wear, fitting connections, and cylinder actuation all create opportunities for small quantities of hydraulic oil to enter the coolant system. This is tramp oil contamination.
The behavior of hydraulic oil when it contacts water-based cutting fluid determines the cost impact of contamination. Conventional hydraulic oils that emulsify readily in water become incorporated into the coolant as a stable dispersion. Emulsified tramp oil cannot be separated by passive methods and degrades cutting fluid performance across several dimensions:
- Reduces concentration effectiveness of semi-synthetic and synthetic cutting fluids, accelerating biocide depletion and creating conditions favorable to bacterial growth
- Forms a stable foam under agitation, reducing heat transfer capacity and causing pump cavitation in high-pressure coolant systems
- Accelerates coolant sump turnover, increasing disposal cost and fluid replenishment frequency
- Increases tool wear rates and raises the incidence of workpiece finish defects
Antiwear 32 does not emulsify in water-based cutting fluids. The oil phase separates from the water phase and rises to the surface, where it can be removed by standard methods including decantation, skimming, coalescing plates, and centrifugal separators. This behavior directly reduces tramp oil management cost in production environments where the hydraulic system and coolant sump share the same machine enclosure.
Semi-synthetic cutting fluids, which represent the most widely used cutting fluid category in general metalworking, are particularly susceptible to emulsified tramp oil degradation. The use of a non-emulsifying hydraulic fluid in the workholding system is the most cost-effective point of control.
Available in pail, drum, and 275-gallon IBC. Order direct from Hangsterfer's Laboratories.
Order Antiwear 32 →
Product Characteristics
The following data is drawn from the Hangsterfer's Antiwear Technical Data Sheet. The complete TDS and Safety Data Sheet are available from Hangsterfer's Customer Resources.
| Property |
Antiwear 32 |
Test Method / Notes |
| ISO Viscosity Grade |
ISO VG 32 |
ISO 3448 |
| Kinematic Viscosity @ 40°C |
30 to 35 cSt |
ASTM D445 |
| Viscosity, SUS @ 100°F |
145 to 160 SUS |
ASTM D2161 |
| Viscosity Index (VI) |
> 95 |
ASTM D2270 |
| Specific Gravity |
0.85 to 0.88 |
ASTM D4052 |
| Flash Point (COC) |
419°F / 215°C |
ASTM D92 |
| Appearance |
Golden |
Visual |
| Odor |
Mild |
Sensory |
Standards and Specifications Compliance
| Specification |
Status |
| ISO VG 32 |
Meets |
| Cincinnati Milacron P-68 |
Meets or Exceeds |
| Cincinnati Milacron P-69 |
Meets or Exceeds |
| Cincinnati Milacron P-70 |
Meets or Exceeds |
| VOC Compliant |
Yes |
| Solvent Free |
Yes |
| REACH Compliant |
Yes |
Health and Safety
Antiwear 32 is formulated without solvents and is VOC compliant. The product carries a mild odor designation across all viscosity grades in the Antiwear series, which is relevant in the enclosed CNC machine tool environment where operator exposure to misting or vapor is a chronic rather than acute consideration.
The product is REACH compliant and is manufactured by an ISO 9001:2015 certified facility. Safety Data Sheets for all Hangsterfer's products are available through their customer portal. Consult the SDS before handling, storing, or disposing of this product.
Dispose of used hydraulic fluid in accordance with applicable local, state, and federal regulations. Used petroleum oils are generally accepted for re-refining or energy recovery.
Order Antiwear 32 from Hangsterfer's
Available in pail, drum, and 275-gallon IBC. Distributor locations on hangsterfers.com.
Order from Hangsterfer's →
This document is provided as a reference guide. Fluid selection must be verified against machine tool OEM requirements and supplier specifications for each installation.
Disclosure: Carr Lane Manufacturing receives a referral credit on qualified outbound clicks to Hangsterfer's Laboratories from this page. Editorial content reflects Carr Lane's independent engineering recommendation; the recommendation is not contingent on referral activity.